Debunking Common Misconceptions About Toxic Gas Detection in Semiconductor Facilities

Learn 5 common misconceptions about toxic gas detection in semiconductor fabs—sensor selection, calibration, alarm thresholds, placement, and integration.

Semiconductor manufacturing is one of the most advanced and demanding industries in the world. It relies on a wide range of specialty gases, many of which are toxic, corrosive, or highly reactive, to enable critical processes like etching, doping, and deposition. While these gases are essential to production, they also pose significant safety and regulatory risks.

Toxic gas detection systems serve as the first line of defense against those risks. Yet misconceptions about how detection systems work can lead to gaps in protection. In some cases, those gaps remain hidden until a minor leak escalates into an unplanned shutdown, regulatory exposure, or a reportable safety incident.

Improving facility readiness begins with understanding potential gaps and correcting them.  In this article, we examine five common misconceptions about toxic gas detection and share best practices to help facilities move from reactive protection toward intentional, risk‑informed safety design.

Quick Summary: Key Takeaways
  • No single sensor detects all gases; different technologies are required.
  • Calibration is critical for accuracy, reliability and compliance.
  • Alarm thresholds must be customized for each gas and process.
  • Detection alone isn’t enough; integrated safety strategies are essential.
  • Gas properties affect sensor placement and detection strategy.
Misconception #1: “One Sensor Technology Detects All Gases”

It’s a common assumption that a single sensor technology can cover every gas used in a semiconductor fab. In reality, toxic and hazardous gases vary widely in their physical and chemical properties, requiring different detection technologies to identify them reliably.

Electrochemical sensors are ideal for gases like chlorine or ammonia, infrared sensors work best for hydrocarbons and carbon dioxide, and photoionization detectors are designed for volatile organic compounds.

Relying on a single technology creates blind spots that can compromise safety. For example, an electrochemical sensor cannot effectively detect silane or arsine. The best approach is to conduct a thorough gas inventory and deploy multi-technology detection systems to improve overall readiness and cover the full range of gases used in your processes.

Misconception #2: “Calibration Is Optional”

Even when the right sensors are installed, their accuracy cannot be taken for granted. Over time, environmental factors such as humidity, temperature changes, and exposure to contaminants can cause sensor drift. Left unaddressed, drift can lead to false negatives, where leaks go undetected, or false positives that trigger unnecessary alarms and operational disruptions.

Regular calibration is essential to maintain accuracy, reliability and compliance. Most manufacturers recommend calibration every six months, using certified calibration gases. In high-volume or high-risk environments, automated calibration systems can help reduce human error while improving efficiency.

Organizations that skip or delay calibration often believe their systems are “covered,” only to discover during audits or assessments that accuracy has quietly degraded.

Misconception #3: “Alarm Thresholds Are Universal”

Alarm thresholds are not one-size-fits-all. They depend on gas toxicity, permissible exposure limits set by organizations such as OSHA or ACGIH, process-specific requirements such as SEMI standards, and local regulatory obligations.

When alarms are set too conservatively, nuisance alarms can become frequent, leading to alarm fatigue and slower response times. When they are set too high, dangerous concentrations may go unaddressed. The most effective approach is to customize alarm thresholds for each gas based on formal risk assessments and to implement tiered alarms that support appropriate escalation and response.

Because processes, gas inventories, and regulations evolve over time, alarm settings should be reviewed regularly as part of an ongoing detection readiness program.

Misconception #4: “Detection Alone is Enough

Detection plays a critical role in protecting personnel and facilities, but it is only one layer of a comprehensive safety strategy. Detection systems cannot prevent harm on their own if they are not integrated with other safeguards.

Effective programs connect gas detection to ventilation controls, interlocks, and automatic shutdowns. They also include clearly defined emergency response procedures, regular training, and drills, so personnel know how to respond when alarms occur. Without these complementary measures, even accurate detection may not translate into effective risk mitigation.

Misconception #5: “All Toxic Gases Behave the Same

Not all gases behave alike. Heavier-than-air gases such as chlorine tend to settle near the floor, while lighter gases like ammonia rise. Some gases adsorb onto surfaces or react with moisture, which can complicate detection and interpretation of readings.

Diffusion rates and airflow patterns also influence how quickly a leak spreads and where it is most likely to be detected. These factors make sensor placement just as important as sensor selection.

Addressing this misconception requires airflow modeling, placement of sensors near likely leak sources and accumulation zones, and periodic reassessment whenever equipment layouts or ventilation patterns change.

Conclusion

Misconceptions about toxic gas detection rarely stem from gaps in training or outdated information.  More often, they result from oversimplified assumptions applied to complex systems. As this article illustrates, effective gas detection is not achieved through a single sensor choice, default alarm settings, or infrequent calibration. It is a continuous, system-level discipline shaped by gas chemistry, facility design, operational practices, and regulatory expectations.

When detection strategies fail to account for sensor limitations, calibration drift, gas-specific thresholds, or real-world gas behavior, even well-intentioned safety programs can develop critical blind spots. In contrast, facilities that approach gas detection as an integrated, evolving safety function are better positioned to protect personnel, maintain compliance, and avoid costly disruptions.

This shift from reactive detection to intentional, risk‑informed design is foundational to facility readiness. By aligning detection strategies with actual process conditions, semiconductor manufacturers can strengthen both safety outcomes and operational resilience. At Honeywell, we support this approach through advanced detection technologies and integrated safety solutions designed to help facilities move beyond misconceptions and toward measurable, sustainable protection.

Take the Facility Readiness questionnaire to uncover hidden detection gaps, benchmark your current approach, and prioritize improvements before they become incidents.